Share license privileges with other users on the network

Share license privileges with other users on the network

Adjust network settings to provide additional privileges to users on the network or to use License Source Protection when using a remote desktop connection.
When sharing license privileges with users on the network consider:
  • Configure the network to allow communication between the devices that need to share license privileges. Set TCP and UDP ports 22350 to open on the computer that provides privileges.
  • Enable the license to share for network use. Use the License Portal to configure licenses and optionally enable them for network use.
  • The computers that receive permissions from the remote workstation must install a CmStick that contains the same license with
    Use
    permission. Plug the CmStick into a USB port locally on the computers.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal