11:30 a.m. - 12:00 p.m. Singapore Time (GMT+8)
9:00 a.m. - 9:30 a.m. India Standard Time (GMT+5:30)
1:30 p.m.-2:00 p.m. Australian Eastern Standard Time (GMT+10)
3:30 p.m.-4:00.p.m. New Zealand Standard Time (GMT+12)
In small-scale process control systems, especially fluid control where sequence control is involved, each step must be coded. Whether the process development can be completed with minimal coding, simple configuration functions and in compliance with the S88 control standard is critical to the efficiency and standardization during process development.
In this webinar, we introduce a Configurable Recipe Sequence Manager that can support the configuration of sequence recipes more flexibly, leading to more successful and consistent results. With lesser coding required, OEM users can benefit from reduced lead times, while end users can seamlessly configure according to their specific process needs. The solution can store multiple recipes, which can be applied to different process requirements.