Micro850 and enhanced Micro830 micro PLC features – including embedded motion control – provide just-enough control flexibility for lower-end applications
MILWAUKEE, Oct. 29, 2012 — To meet machine builders’ needs for flexible micro programmable logic controllers (PLCs) that optimize stand-alone machine performance and cost, Rockwell Automation announces the new Allen-Bradley Micro850 and enhanced Micro830 PLCs. Both micro PLCs feature embedded motion capabilities for up to three axes of motion, allowing them to support a wide range of applications.
“To be profitable, machine builders around the globe demand world-class micro PLCs,” said Co Gia Nguyen, vice president and general manager, Rockwell Automation Asia Pacific Business Center. “But these controllers must meet machine builders’ requirements for economical, just-enough control, while providing additional options and features that enable machine builders to differentiate their machines from the competition. The new Micro850 and enhanced Micro830 controllers balance those needs and help machine builders compete more profitably.”
The Micro850 micro PLC is equipped with the same form factor, plug-in support, instruction/data size and motion capabilities as the 24-pt and 48-pt Micro830 controllers, but with the added capabilities of Ethernet and expansion I/O. The Micro850 controller specifically targets the needs of OEMs and excels at stand-alone machine applications.
The Micro850 controller has an embedded Ethernet port for higher performance connectivity to human-machine interfaces (HMIs). The EtherNet/IP protocol with CIP Symbolic support is used for simplified Allen-Bradley PanelView Component HMI connectivity. Tags created while configuring the HMI screens can easily reference the variable names in the Allen-Bradley Micro800 program.
I/O flexibility in the Micro850 PLC is one of the keys to successfully minimizing the cost of a machine. With support for up to five plug-ins, OEMs can customize the functionality of the controller with additional I/O, special functions, and serial ports without increasing the size of the controller. If more I/O or higher-performance analog I/O is required, the Micro850 controller supports up to four 2085 expansion I/O modules, including high-density digital I/O and high-accuracy analog I/O, for a total of 132 digital I/O points.
The enhanced Micro830 (via a firmware and software upgrade) and Micro850 controllers support up to three motion axes using pulse output to stepper or servo drives. OEMs can use intuitive motion function blocks, including Home, Move Velocity, Move Absolute, and Move Relative to make single-axis moves easy. For applications where precise positioning is required at high speeds, the Touch Probe function block has special hardware to achieve exact-position registration.
A single programming software called Connected Components Workbench simplifies the installation, configuration, connectivity, and maintenance of machine devices, including the series of Micro800 controllers, Allen-Bradley PowerFlex AC drives, and PanelView Component graphic terminals. The single Connected Components Workbench software saves OEMs time and associated costs compared with using a different programming tool for each device.
For more information on the Micro800 family of PLCs and Connected Components Workbench software, visit http://www.ab.com/programmable-controllers/micro800 or contact your local Allen-Bradley distributor.
About Rockwell Automation
Rockwell Automation, Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable.
Headquartered in Milwaukee, Wis., Rockwell Automation employs over 21,000 people serving customers in more than 80 countries.
For more information:
- Micro850 and Micro830 programmable logic controllers: http://ab.rockwellautomation.com/Programmable-Controllers/Micro800
- Micro850 photo: http://flic.kr/p/diLyQj
- Micro830 photo: http://flic.kr/p/diP6xT
- Micro850 video: http://youtu.be/Tgr1BT2fvXY
- Micro830 video: http://youtu.be/6cVeQYp-MQM
Media contacts:
Sarah Larson
Rockwell Automation
414.382.5910
selarson@ra.rockwell.com
Patty Hoffman
Padilla Speer Beardsley Inc.
612.455.1781
phoffman@padillaspeer.com
Allen-Bradley, Connected Components Workbench, LISTEN. THINK. SOLVE., Micro800, Micro830, Micro850, PanelView and PowerFlex are trademarks of Rockwell Automation, Inc.
CIP and EtherNet/IP are trademarks of ODVA.
# # # #
Published October 28, 2012