Manually tune an axis
Use the
Manual Tune
dialog box to manually tune gains for optimum drive servo loop performance. Perform a manual tune if the software calculation defaults and the Autotune results are not acceptable. Changes to the data in the panel are immediately committed. Before you begin:
- In theGeneralpage, in theAxis Configurationbox, selectPosition LooporVelocity Loop. Manual tuning only applies to these two application types.
To manually tune an axis:
- Access theManual Tunedialog box:
- Right-click the axis in the motion group and clickManual Tune.
- ClickManual Tuneon the bottom of theAxis Propertiesdialog box.
- InSystem Bandwidth, type a value or move the slider to enter the overall bandwidth of the drive's servo loop.
- InSystem Damping, type a value or move the slider to enter the overall damping of drive's servo loop.
- In Tuning Configuration, click + to display the currentApplication Type,CouplingandGains to Tunesettings.
- If theAxis Configurationis set toPosition Loop, underPosition Loop, configure the position loop and integrator bandwidth, select to enable or disable the integrator hold and the error tolerance for the position loop.
- If theAxis Configurationis set toVelocity Loop, underVelocity Loop, configure the velocity loop and integrator bandwidth, select to enable or disable the integrator hold and the error tolerance for the velocity loop.
- ClickAdditional Tuneto configure feedforward, compensation, filters, limits and planner tuning options.
- ClickResetto return the values to the state they were in at the time the Manual Tune dialog box opened.
Provide Feedback