Module Properties - Associated Axes
Use this tab to configure the selected SERCOS motion modules by associating axis tags, of the type AXIS_SERVO_DRIVE, with nodes available on the module. Use this tab to configure these SERCOS motion modules:
- 1394 SERCOS Interface Drives
- 2094Kinetix6000 Drive
- Kinetix6200 Drive
- 2098Ultra3000 SERCOS Drive
- 8720MC SERCOS Drive
Parameters
Node
Displays the selected node of the
Ultra™
3000, Kinetix®
6000, Kinetix
6200, or 8720MC drive, as selected on the General tab. This field allows you to associate an AXIS_SERVO_DRIVE tag with the drive’s node.
TIP:
This field is read-only while you are online.

Click this button to access the Axis Properties dialog for the associated axis.
New Axis
Click this button to navigate to the New Tag dialog to create an AXIS_SERVO_DRIVE tag to associate with one of the nodes.
OK
Click this button to accept your edits and close the dialog.
Cancel
Click this button to cancel your edits and close the dialog.
Apply
Click this button to apply your edits and continue editing.
Help
Click this button for help on this tab.
Provide Feedback