Loading
CASE STUDY | FOOD & BEVERAGE
Recent ActivityRecent Activity
4 minute read

PFi’s new Australian-made Titanium Cross Flow Membrane Wastewater Solution

New innovation reduces downtime, increases yield, and lowers environmental footprint

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
PFi’s new Australian-made titanium cross flow membrane wastewater solution.
Products For Industry (PFi) Logo

Products For Industry (PFi) is a locally owned and operated business servicing the industrial sector. PFi is proud to offer a full suite of in-house capabilities to support manufacturers with machine automation products, systems, and solutions.

From small workshop engineering requirements through to complete factory automation upgrades, PFi ensure clients are fully supported from concept through to production.

Challenge
  • PFi’s new titanium cross flow membrane solution for wastewater treatment needed automation hardware that was streamlined, repeatable, and easy to integrate.
  • Customer specified that the coding style needed to be PAC-ML, an internationally recognised standard
  • PFi needed a solution that would gain strong market acceptance when entering export market
Solution
  • CompactLogix™ Control System
  • PanelView Plus™ Graphic Terminal
Result
  • CompactLogix controllers provide higher performance, increased capacity, improved productivity, and enhanced security to help meet growing demands of smart machines and equipment for manufacturing.
  • PanelView Plus provides the graphical interface through a seamless integration with the CompactLogix Controller. This integration enables engineers to enter configuration information once and use it for the entire automation design. It also helps build modern applications with high-speed HMI buttons for jogging applications, scalable vector graphics, and a pre-configured system banner that provides diagnostic information.

Challenge

Australian innovator, Products For Industry (PFi), is introducing what is believed to be a world-first pure titanium cross flow membrane solution, which has uptime, environmental, and yield benefits compared to traditional wastewater treatment methods.

After more than 10 years of development, this fully evolved and tested product is now entering service in Australia with a leading beverages company, which will use the new technology to separate solids from liquid streams in various stages of the waste stream process.

“This solution is game-changing for the food and beverage industry, particularly beverages and spirits, because titanium allows for a lower footprint, and longer times between Clean In Place (CIP), thereby reducing downtime,” said PFi managing director, Gavin Dunwoodie.

PFi is a locally-owned and operated business servicing the industrial sector, offering a full suite of in-house capabilities to support manufacturers with machine automation products, systems and solutions, from concept through to production.

“With traditional membranes made of ceramic or plastic, back-pulsing and cleaning often creates problems, so the overall lifetime of the equipment is reduced,” added Dunwoodie.

Titanium (Ti) is the ninth most known metal in the earth’s crust and possesses the highest strength-to-weight ratio. It is as strong as steel, but weighs 45% less, and is non-magnetic, non-corrosive, and does not conduct electricity.

“This forward-thinking beverages company wanted an advanced solution that would continue to increase their throughput, while lowering their environmental footprint. They were clear from the outset that there should be no compromises on quality,” said Dunwoodie.

Solution

Simple integration of automation hardware

“We needed automation hardware that was streamlined, repeatable, and easy to integrate, so we selected Rockwell Automation’s CompactLogix™ Control System and PanelView Plus™ Graphic Terminal. These provided us with a premium integration that would be accepted by global leaders like this beverages company,” said Dunwoodie.

Rockwell Automation’s CompactLogix controllers provide higher performance, increased capacity, improved productivity, and enhanced security to help meet the growing demands of smart machines and equipment for manufacturing.

PanelView Plus provides the graphical interface through a seamless integration with the CompactLogix Controller. This integration enables engineers to enter configuration information once and use it for the entire automation design. It also helps build modern applications with high-speed HMI buttons for jogging applications, scalable vector graphics, and a pre-configured system banner that provides diagnostic information.

“Rockwell worked with us to select the best hardware for the job, made sure it was fit-for-purpose, and supported us along the way,” said Dunwoodie.

“Additionally, the customer specified that the coding style needed to be PAC-ML, an internationally recognised standard, so Rockwell set up its technologies to match this need,” he added.

Rockwell Automation regional director, South Pacific, Anthony Wong, said, “We are delighted to be able to provide automation technology solutions, and ongoing support for PFi’s latest Australian innovation. PFi is a valued Gold OEM partner in our PartnerNetwork™, and we look forward to our continued collaboration to add value to customers.”

Result

Australian innovation

To develop the titanium cross flow membrane solution, PFi built a new factory on its existing site in Queensland.

“We conducted extensive pilot tests at a wastewater treatment plant in New Zealand three years ago, where we found the titanium solution allowed very high flow and flux rates, easy and fast CIP, and no fouling or long-term issues with fats, oils, and greases (FOG). It also showed us that running costs and energy use would be reduced over the system’s lifetime, and the titanium membrane can be 100% recycled at the end of its use in the solution,” said Dunwoodie.

“We also appreciate the support we received from the Australian Government, to help scale up and accelerate the success of this product, which has considerable local and export potential,” he added.

Solution advantages

With titanium’s natural advantages as a material, its use in a cross flow membrane comes with several advantages, including:

  • A continuous length of more than 1.3m
  • A larger range of apertures and filtration sizes are possible
  • Wall thicknesses below 400 Microns are possible, which PFi believes to be unique globally
  • Higher levels of resistance to temperature, acidity, and pressure
  • Industry-leading high flux rates and flow levels through the membrane
  • Materials are non-perishable and recyclable
  • The tube density and surface area per housing is industry leading
  • It is back-pulsable, steam-cleanable, and chemical resistant. Ceramic membranes cannot be back-pulsed, and the cost is comparable to this new titanium alternative
  • Longer times are possible between CIP, which reduces downtime
  • Lower footprint, lower energy consumption, and greater product life

Scalability

Dunwoodie sees great potential for this solution globally, and is looking to scale up operations, after successful pilots, testing, and now in service with this beverages giant.

“Rockwell’s standard design will help with our solution’s market acceptance when we enter the export market. There is particularly strong potential in the spirit industry, where it can replace paper membranes to deliver better outcomes with reduced waste,” he said.

“Titanium provides a true closed loop solution, as the only 100% recyclable membrane, even after 20 or more years in service, which is an outstanding benefit to an end-user’s ESG goals.”

Published December 9, 2024

Topics: Accelerate Digital Transformation Drive Sustainability Food & Beverage Water Wastewater Industrial Control Products
Subscribe to Rockwell Automation

Receive the latest news, thought leadership and information directly to your inbox.

Subscribe now

You may also be interested in

Loading
Loading
Loading
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Com... Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Case Studies Chevron RightChevron Right
  5. Chevron LeftChevron Left Rockwell Automation Powers PFi’s Australian Wastewater Solution Chevron RightChevron Right
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
You can update your preferences at any time. For more information please see our Privacy Policy
CloseClose