19-inch rack-mount design provides centralized point of network distribution and increased port density
MILWAUKEE, Sept. 28, 2015 — Rockwell Automation has expanded its portfolio of industrial Ethernet switches with the new Allen-Bradley Stratix 5410 industrial distribution switch. With four 10-gigabit Ethernet ports, the Stratix 5410 switch provides a high-performance connection to the rest of a facility’s network architecture. The switch can be used as a Layer 2 switch or a Layer 3 routing switch, which allows engineers to use it in various applications.
“Our expanded Stratix family of switches gives IT and engineering professionals the broad range of switches they need for high-availability network designs,” said Mark Devonshire, product manager for Rockwell Automation. “The Stratix 5410 distribution switch offers the performance and flexibility needed for designing future-ready network architectures.”
With a 19-inch rack-mount design, the Stratix 5410 switch gives end users a centralized point of network distribution and increased port density. It is ideal for heavy industry applications where resiliency is often required, and has a rugged exterior to help withstand harsh environmental conditions.
With embedded Cisco technology and Premier Integration into the Rockwell Automation Integrated Architecture system, the Stratix 5410 switch provides familiar solutions for information technology (IT) and operations technology (OT) professionals. This helps ease network configuration, management and support. Using the Rockwell Software Studio 5000 design environment, engineers can leverage FactoryTalk View faceplates from Rockwell Automation and add-on profiles to simplify switch configuration and monitoring. In addition, the embedded Cisco technology helps optimize integration with the enterprise network.
Enhanced security features include programmable port access, as well as configurable port security. Capabilities such as encrypted administrative traffic, 802.1x authentication, access control lists (ACL), and TACACS+ and RADIUS support plantwide security as part of a defense-in-depth security approach.
News Release Assets
Image available upon request or here at box.com.
About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs about 22,500 people serving customers in more than 80 countries.
Media Contacts
Tiffany Pfremmer
Rockwell Automation
414.839.7425
tbockhop@ra.rockwell.com
Leanne Hanson
PadillaCRT
612.455.1776
leanne.hanson@padillacrt.com
Allen-Bradley, FactoryTalk, Integrated Architecture, LISTEN. THINK. SOLVE., Rockwell Software, Stratix, Stratix 5410 and Studio 5000 are trademarks of Rockwell Automation Inc.
Published September 27, 2015