Elasticsearch Logs

Elasticsearch Logs

The Elasticsearch Logs are enabled by default and are available in the path specified while installing Elasticsearch. Refer the Fig. 4-30 screenshot.
TIP:
Unhide the hidden files. In the View menu, select the [Hidden items] checkbox. The hidden files display.
Hidden Files
<<Elasticsearch Installation <DataView_HOME>>
> Program Data>Elastic>Elasticsearch>logs
Elasticsearch Log
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal