Extractors

Extractors

Extractors connect to source systems and push data in its original format to Cognite Data Fusion (CDF) as part of the data integration workflow. In FactoryTalk DataMosaix, you can extract data by registering an extractor from the available source types to extract data.
You can also create custom extractors if your source type cannot be use with any of the available extractors. Select a custom extractor to get started.
NOTE:
In Extractors, the optional parameter can be set to either an empty value or null.
First-Time Extractor Creation
When you create an extractor for the first time, to get a concise introduction and understand extractors better, click
First Time Overview
located in the top left corner of the Extractor Info Detail page. While configuring the extractor, you'll also find Learn More [] icon within each section (General Info, Pipeline, and Source Info). When you click on these icons, a quick overview specific to each section will be displayed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal