Smart Object properties
These are the Smart Object properties.
Element | Description |
Desc | Description. Information that describes the Smart Object. |
Version | Version information for the Smart Object. String formatted as major.minor.build. Each revision number can be 0 to 999. If there is no period, the number is treated as a major revision only. |
Provide Feedback