Configure multiple devices

When you add multiple devices at the same time, you can configure basic settings for the devices all at once.
To configure multiple devices
:
  1. In
    Devices
    explorer, select Hamburger Menu
    Hamburger Menu
    , then select Add device icon
    Add device
    . The
    Add device
    dialog box opens.
  2. Select each catalog number to add to the project. The selected devices appear in the
    Devices to Add
    list on the right of the dialog.
  3. Select
    Continue
    . The
    Bulk Configure
    dialog opens.
  4. Configure basic properties for each device to add it to the project. The basic properties vary depending on the device type.
    • Device name
      . Enter a unique name for the device.
    • Chassis size
      . Select the number of slots in the chassis.
    • Slot number
      . Select a slot for the device.
    • IP address
      . Enter an IP address for the device.
  5. Select
    Finish
    . When the devices are added to the project, they are listed in the
    Devices
    explorer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.