Set options

Set options

Specific global settings for the
FactoryTalk Optix Studio
software.
Global settings include the language displayed on the user interface, activation of the log messages, activation of features under development, the default code editor for any Netlogic C# code, the unit of measurement for physical lengths, and version control settings.
  1. In the
    FactoryTalk Optix Studio
    title bar, select the drop-down arrow after
    FactoryTalk Optix Studio
    Options
    and select
    FactoryTalk Optix Studio Options
    .
  2. In
    FactoryTalk Optix Studio Options
    , complete:
    • Language
      . Select the language for the user interface.
    • Advanced mode
      .  Activate the advanced log messages displayed in the
      Output
      pane.
    • Show feature previews
      . Activate
      FactoryTalk Optix Studio
      features that are under development and may create instability in projects.
    • Preferred code editor
      . Set the default code editor for any NetLogic C# code
    • Preferred physical length unit
      . Set the default unit of measurement for physical lengths.
  3. Under
    Version Control User Configuration
    , complete:
    • User Name
      . The username of the logged in user account when a project is stored in a version control repository.
    • User Email
      . The email address of the logged in user account when a project is stored in a version control repository.
  4. Under
    Version control providers and IDs
    , in
    Select a provider
    , select the username authorized to store projects in the version control repository and then select
    Add identity
    .
  5. Select
    Save
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.