- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Create an alarm grid
Create an alarm grid that displays color-coded and selectable alarm events.
TIP:
You can use a preconfigured alarm grid instead of creating it from scratch. For more information, select
and select .
Template Libraries
- Create a panel for the alarm grid and controls:
- InProject view, right-clickMainWindow (type)and select .
- Hover-over the panel, select, and enterAlarmGridPanel.
- Create and configure a data grid for alarms:
- InProject view, right-clickAlarmGridPaneland select .
- Hover-over the data grid, select, and enterAlarmsGrid.
- InProperties, create a dynamic link between theModelproperty and .TIP: You can select thevalues from the@AttributeAttributedrop-down menu at the bottom of the dialog.For more information about dynamic links, see Create dynamic links.
- ExpandModeland create a dynamic link betweenItemKindandFor more information about dynamic links, see Create dynamic links.
- SetSort ordertoDescending.
- Create four alarm grid text columns:
- Next toColumns, selectand selectText column.
- Rename the columns by hovering-over each column, selecting, and entering:
- TimestampColumn
- NameColumn
- SourceVariableColumn
- MessageColumn
- SeverityColumn
- Create three alarm grid image columns:
- Next toColumns, selectand selectText column.
- Rename the columns by hovering-over a column, selectingand entering:
- ActiveColumn
- AcknowledgedColumn
- ConfirmedColumn
Provide Feedback