Keyboards

Keyboards

Add virtual keyboards in your project to provide touch input for operators. Configure the Keyboard object to define custom virtual keyboards.

Keyboard engine types

Available virtual keyboard engines:
Built-in
The default virtual keyboard that is available only for the native presentation engine.
Custom
Customizable virtual keyboard that is available for both the native presentation engine and web presentation engine. For more information, see Configure a custom keyboard.
None
No virtual keyboard.
You configure the virtual keyboards for the project by adjusting presentation engine properties. For more information, see Select a keyboard.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.