- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Create a project template
Create a project template to contain the default content for projects that are based on the
template. Create the template from an existing project. New projects that you create based on
the template contain the content of the template by default.
- Add the content that you want to appear as default content in projects that you create with the template.
- From the toolbar, select the down arrow afterSaveand selectSave As.
- In Save project as, complete:
- Name. Enter the new name of the project.
- Location. Type the path where you want to save the project. Select and browse a folder to navigate to the location.
- Template. Select to save the project as a template.
- (optional) Use Version Control. Select to track changes made to the project and store the project in a Git repository.
- (optional)Encrypt secrets. Select to encrypt sensitive data contained in projects.
- SelectOK.
Provide Feedback