- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Compare committed changes
Compare two different versions of a project by selecting two different committed
changes in
View history
.- From the toolbar, select.View history
- InVersion history, two different commits to compare.TIP: The differences between the commits are highlighted.
- (optional) To toggle the content that appears inVersion history, select either:
- All. Toggle to show all content in the project.
- Updates. Toggle to show only the differences between the selected commits. This is the default.
history
compare
Provide Feedback