- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Edge App Broker
The Edge App Broker facilitates communication between
FactoryTalk Optix
and other applications or external system.The following applications are available:
- Product Quality tracking
- Overall Operations Effectiveness (OEE)
- Sequence Analyzer
- Thingworx connector
- Kafka connector
- MQTT connector
- Web API connector
- Azzure IOT hub connector
- Python execution engine
edge
edge app
edge app broker
Provide Feedback