- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Getting started
Become familiar with the terminology, design concepts, and workflows present in the
FactoryTalk® Optix™
environment and create your first project.Learn about
FactoryTalk Optix
components, FactoryTalk Optix Studio
interface, and basic concepts. See FactoryTalk Optix overview.Configure
FactoryTalk Optix Studio
options and set log levels. See FactoryTalk Optix Studio configuration.Develop and run your first project. See Quick start project.
Provide Feedback