- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
FactoryTalk Optix Studio CLI
Use the command-line interface (CLI) of
FactoryTalk Optix Studio
to perform
actions without having to interact with the graphical user interface (GUI).
TIP:
Running CLI commands is useful for scripting and
automating pipelines.
To run a command, see Run a CLI command. To learn about the
available commands, see CLI commands.
Provide Feedback