- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Publish the object
Add an OPC UA server and publish the object that exposes an OPC UA
method.
- InProject view, right-clickOPC-UAand select .OPCUAServerappears underOPC-UA.
- InProperties, next toNodes to publish, select.A configuration of nodes to be published appears underNodes to publish.
- UnderConfiguration1, next toNodes, select.
- FromProject view, dragMyObject1next toNode1inProperties.
- (optional) Adjust other OPC UA server preferences. See Add an OPC UA server.
Provide Feedback