- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
File Standard Deviation (STD)
This table lists the controllers and applications that support this instruction.
Architecture | Standard applications | Safety applications |
---|---|---|
CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers | Yes | No |
CompactLogix 5380, CompactLogix 5480, ControlLogix 5580, Compact GuardLogix 5380, and GuardLogix 5580 controllers | Yes | Yes |
The STD instruction calculates the standard deviation of a set of values in one dimension of the Array and stores the result in the Destination.
Available Languages
Ladder Diagram
Function Block
This instruction is not available in function block.
Structured Text
This instruction is not available in structured text.
Operands
There are data conversion rules for mixed data types within an instruction. See Data Conversion.
Ladder Diagram
Operand | Type | Format | Description |
---|---|---|---|
Array | SINT INT DINT REAL | array tag | Find the standard deviation of the values in this array specify the first element of the group of elements to use in calculating the standard deviation |
Dimension to vary | DINT | immediate (0, 1, 2) | which dimension to use the order of the dimensions is: array[0,1,2] |
Destination | REAL | tag | result of the operation |
Control | CONTROL | tag | Control structure for the operation |
Length | DINT | immediate | number of elements of the array to use in calculating the standard deviation |
Position | DINT | immediate | Offset into the specified array which identifies the current element that the instruction is accessing.
initial value is typically 0 |
Length and Position (corresponding to .LEN and .POS in the control tag) are pseudo-operands. For details, see Pseudo-operand initialization.
CONTROL Structure
Mnemonic | Data Type | Description |
---|---|---|
.EN | BOOL | The enable bit indicates the STD instruction is enabled. |
.DN | BOOL | The done bit is set when the instruction has operated on the last element in the Array. |
.ER | BOOL | The error bit is set when the instruction generates an overflow. The instruction stops executing until the program clears the .ER bit. The .POS value stores the position of the element that caused the overflow. |
.LEN | DINT | The length word specifies the number of elements in the array on which the instruction operates. |
.POS | DINT | The position word is an offset into the specified array which identifies the current element that the instruction is accessing. |
Description
The standard deviation is calculated according to this formula:
Where:
start = dimension-to-vary subscript of the array operand
xi = variable element in the array
N = number of specified elements in the array
AVE =
IMPORTANT:
Make sure the Length does not cause the instruction to exceed the specified Dimension to vary. If this happens, the Destination will be incorrect.
If an overflow occurs during expression evaluation or if the instructions reads past the end of an array, the instruction sets the ER bit and stops execution.
Affects Math Status Flags
Controllers | Affects Math Status Flags |
---|---|
CompactLogix 5380, CompactLogix 5480, ControlLogix 5580, Compact GuardLogix 5380, and GuardLogix 5580 controllers | Conditional, based on programming language. See Math Status Flags. |
CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers | Yes |
Major/Minor Faults
A major fault will occur if: | Fault type | Fault code |
---|---|---|
.POS < 0 or .LEN < 0 | 4 | 21 |
Dimension to vary > number of dimensions | 4 | 20 |
See Common Attributes for operand-related faults.
Execution
Ladder Diagram
Condition / State | Action Taken |
---|---|
Prescan | The .EN bit is cleared.
The .DN bit is cleared.
The .ER bit is cleared. |
Rung-condition-in is false | The .EN bit is cleared.
The .ER bit is cleared.
The .DN bit is cleared. The .POS value is cleared.
The rung-condition-out is false. |
Rung-condition-in is true | Internally, the instruction uses a FAL instruction to calculate the average: Expression = standard deviation calculation Mode = ALL |
Postscan | N/A. |
Examples
Example 1
Calculate the standard deviation of arrayDint, which is DINT[4,5].
Ladder Diagram
Example 2
Calculate the standard deviation of dint_array, which is DINT[4,5].
Ladder Diagram
Provide Feedback