Access Attributes from Ladder Logic
You can find attributes that are accessible through SSV or GSV instructions in Ladder Logic. There are three main categories of attributes: status, interface, and configuration.
The GSV/SSV access is filtered based on the axis configuration type - Position Loop, Velocity Loop, Torque Loop, Feedback.
For example,
Axis Configuration Type | Attribute Available |
---|---|
Position Loop | PositionLoopBandwidth
VelocityLoopBandwidth |
Velocity Loop | VelocityLoopBandwidth (only) |
Torque Loop | Neither attribute is available. |
Provide Feedback