- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Motor Test Result Attributes
These are the attributes that are associated with result status applied to a Motion Control Axis.
Motor Test Status
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - D | Get/GSV | USINT | - | - | - | Enumeration: 0 = test process successful 1 = test in progress 2 = test process aborted 3 = test process timed-out 4 = test process faulted 5 = test reached travel limit 6 = reserved 7 = test measurement error 8 = test configuration error 9-127 = reserved 128-255 = vendor specific 128= test prohibited - axis test mode active |
The Motor Test Status attribute returns status of the last Run Motor Test service on the targeted drive axis. The Motor Test Status attribute can be used to determine when the motor test service has successfully completed. Conditions may occur, however, that make it impossible for the drive to properly perform the operation. When this is the case, the test process is automatically terminated and a test error is reported that is stored in the Motor Test Status output parameter. Values in the normal vendor specific range (128-255) correspond to values defined in the vendor-specific range in the open service on the device.
Motor Test Resistance
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - D | Get/GSV | REAL | - | - | - | Ohms |
This floating point value represents the stator resistance of an induction or permanent magnet motor as measured by the Motor Test procedure.
Motor Test Inductance
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - D IM, SPM only | Get/GSV | REAL | - | - | - | Henries |
This floating point value represents the motor inductance of an induction or permanent magnet motor as measured by the Motor Test procedure.
Motor Test Flux Current
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - D IM Only | Get/GSV | REAL | - | - | - | Amps |
This floating point value represents the motor flux current of an induction motor as measured by the Motor Test procedure.
Motor Test Slip Speed
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - D IM Only | Get/GSV | REAL | - | - | - | RPM: rotary motor type m/s: linear motor type |
This floating point value represents the slip speed of an induction motor as measured by the Motor Test procedure.
Motor Test Counter EMF
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - D PM Only | Get/GSV | REAL | - | - | - | Volts |
This floating point value represents the measured Counter EMF (CEMF) of a PM motor at Rated Speed by the Motor Test procedure.
Motor Test Lq Inductance
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - D IPM Only | Get/GSV | REAL | - | - | - | Henries |
This floating point value represents the phase-to-phase q-axis motor inductance measured by the Motor Test procedure.
Motor Test Ld Inductance
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - D IPM Only | Get/GSV | REAL | - | - | - | Henries |
This floating point value represents the phase-to-phase d-axis motor inductance measured by the Motor Test procedure.
Motor Test Lq Flux Saturation
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - D IPM Only | Get/GSV | REAL [8] | - | - | - | % Nominal Inductance |
This floating point value represents the phase-to-phase q-axis stator inductance of the motor as measured by the Motor Test procedure expressed as a percentage of the measured Nominal Inductance, Lq, at 25%, 50%, 75%, 100%, 125%, 150%, 175% and 200% rated continuous current.
Motor Test Ld Flux Saturation
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - D IPM Only | Get/GSV | REAL | - | - | - | % Nominal Inductance |
This floating point value represents the phase-to-phase d-axis stator inductance of the motor as measured by the Motor Test procedure expressed as a percentage of the measured Nominal Inductance, Ld, at 100% rated continuous current.
Motor Test Bus Overvoltage Speed
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - D IPM Only | Get/GSV | REAL | - | - | - | RPM (rotary motor type) m/s (linear motor type) |
This floating point value represents the maximum speed of the motor without exceeding the operational DC bus overvoltage limit, as determined by the Motor Test procedure.
Motor Test Commutation Offset Comp
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - D IPM Only | Get/GSV | REAL | - | - | - | Electrical Degrees |
This floating point value represents the change in motor Commutation Offset at rated continuous current as measured by the Motor Test procedure.
Motor Test Flux Saturation
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - D SPM Only | Get/GSV | REAL[8] | - | - | - | % Nominal Inductance |
Array of measured phase-to-phase stator inductance of the motor as a percentage of the measured Nominal Inductance, PM Motor Inductance, at 12.5%, 25%, 37.5%, 50%, 62.5%, 75%, 87.5% and 100% of the Peak Current Rating.
Provide Feedback