Clutch Brake Wiring-Program Example

The following examples illustrate the use of some of the Metal Form instructions in a press safety application, including the three Clutch Brake instructions (CBIM, CBSSM, and CBCM), the Camshaft Motion Monitor (CSM), and the Crankshaft Position Monitor (CPM).
Wiring Diagram
CSM Clutch Brake Wiring and Program Example
Programming Diagram
CSM Programming Diagram
CSM Programming Diagram 2
Ladder Diagram
CSM Ladder Diagram Example 2_v31
CSM Ladder Diagram Example 1_v31
CBexampleladder3_v31
The programming software is used to configure the input and test output parameters of the
Guard I/O
module, as shown.
Module Definition
RSL5K_ClutchBrake_ModuleDef_v31
Rockwell Automation suggests selecting
Exact Match
from the
Electronic Keying
list. You can also select
Compatible Match
.
Module Input Configuration
RSL5K_CSM Example Module Input Config_v31
Module Test Output Configuration
RSL5K_CSM Example of Module Test Output Config_v31
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.