Motion Axis Fault Reset (MAFR)

Motion Axis Fault Reset (MAFR)

This information applies to the
CompactLogix
5370,
ControlLogix
5570,
Compact GuardLogix
5370,
GuardLogix
5570,
Compact GuardLogix
5380,
CompactLogix
5380,
CompactLogix
5480,
ControlLogix
5580, and
GuardLogix
5580 controllers. Controller differences are noted where applicable.
Use the Motion Axis Fault Reset (MAFR) instruction to clear all motion faults for an axis. This is the only method for clearing axis motion faults.
IMPORTANT:
The MAFR instruction removes the fault status, but does not perform any other recovery, such as enabling servo action. In addition, when the controller removes the fault status, the condition that generated the fault(s) may still exist. If the condition is not corrected before using the MAFR instruction, the axis immediately faults again.
Architecture and safety support
Architecture
Standard
Safety
CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers
Yes
No
Compact GuardLogix 5380, CompactLogix 5380, CompactLogix 5480, ControlLogix 5580, and GuardLogix 5580 controllers
Yes
No
Available Languages
Ladder Diagram
L5K_MAFR_LD_avail_v36
Function Block
This instruction is not available in function block.
Structured Text
MAFR(Axis,MotionControl);
The operands are the same as those for the relay ladder MAFR instruction.
Operands
Ladder Diagram and Structured Text
Operand
Type
CompactLogix
5370,
Compact GuardLogix
5370,
Compact GuardLogix
5380,
CompactLogix
5380,
CompactLogix
5480
Type
ControlLogix
5570,
GuardLogix
5570,
ControlLogix
5580, and
GuardLogix
5580 controllers
Format
Description
Axis
AXIS_CIP_DRIVE
AXIS_CIP_DRIVE
AXIS_GENERIC
AXIS_GENERIC_DRIVE
AXIS_SERVO
AXIS_SERVO_DRIVE
Tip:
AXIS_GENERIC is supported by the
ControlLogix
5570 and the
GuardLogix
5570 controllers only.
Tag
Name of the axis on which to perform the operation.
For controllers that support the REF_TO motion data types, the supported axis operand type can be replaced by an equivalent REF_TO type.
REF_TO_AXIS_CIP_DRIVE
REF_TO_AXIS_VIRTUAL
REF_TO_AXIS_GENERIC
REF_TO_AXIS_GENERIC_DRIVE
REF_TO_AXIS_SERVO
REF_TO_AXIS_SERVO_DRIVE
Reference to the axis on which to perform the operation.
Motion Control
MOTION_INSTRUCTION
MOTION_INSTRUCTION
Tag
Structure used to access instruction status parameters.
MOTION_INSTRUCTION Structure
Mnemonic
Description
.EN (Enable) Bit 31
It is set when the rung makes a false-to-true transition and remains set until the servo message transaction is completed and the rung goes false.
.DN (Done) Bit 29
It is set when the axis’ servo action has been successfully disabled and the drive enable and servo active status bits have been cleared.
.ER (Error) Bit 28
It is set to indicate that the instruction detected an error, such as if you specified an unconfigured axis.
Description
The MAFR instruction directly clears the specified fault status on the specified axis. It does not correct the condition that caused the error. If the condition is not corrected prior to executing the MAFR instruction the axis could immediately fault again giving the appearance that the fault status was not reset.
This instruction is most commonly used as part of a fault handler program, which provides application specific fault action in response to various potential motion control faults. Once the appropriate fault action is taken, the MAFR instruction can be used to clear all active fault status bits.
IMPORTANT:
The .DN bit is not set immediately. It is set once the appropriate Motion module or drive completes its required resets, which could take up to several seconds. Once set the axis is in the Ready state, but only after the request is completed.
In this transitional instruction, the relay ladder, toggle the Rung-condition-in from cleared to set each time the instruction should execute.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. A major fault can occur if an uninitialized reference or a reference of the incorrect type is passed to the Axis operand. See
Common Attributes
for operand-related faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
The .EN, .DN, and .ER are cleared to false.
Rung-condition-in is false
The .EN bit is cleared to false if the .DN or .ER bit is true.
Rung-condition-in is true
The .EN bit is set to true and the instruction executes. If the EN bit is set to false, then there is no action taken.
Postscan
N/A
Structured Text
Condition/State
Action Taken
Prescan
See Prescan in Ladder Diagram table.
Normal execution
See Rung-condition-in is false, followed by rung is true in the Ladder Diagram table.
Postscan
See Postscan in Ladder Diagram table.
Error Codes
See
Motion Error Codes (.ERR)
for Motion Instructions.
Extended Error Codes
Extended Error Codes provide additional instruction specific information for the error codes that are generic to many instructions. See
Motion Error Codes (.ERR)
for Motion Instructions.
MAFR Changes to Status Bits
None
Example
When the input conditions are true, the controller clears all motion faults for myAxis.
Ladder Diagram
Ladder Diagram
Structured Text
MAFR(myAxis,myMotionControl);
Example
When the input conditions are true, the controller clears all motion faults for Axis3.
Relay Ladder
Relay Ladder
Structured Text
MAFR(Axis3,MAFR_3);
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal