IMC Function Block Tuning Errors
If an error occurs during the tuning procedure, the tuning is aborted, and the AtuneStatus bit is set. You can abort the tuning by setting the AtuneAbort bit.
After an abort, the CV will assume its value before the step change, and the GainTuned, TCTuned, DTTuned, and RespTCTuned parameters are not updated. The AtuneStatus parameter identifies the reason for the abort.
Provide Feedback