Emergency Stop (ESTOP)

Emergency Stop (ESTOP)

This instruction applies to the Compact GuardLogix 5370, GuardLogix 5570, Compact GuardLogix 5380, and GuardLogix 5580 controllers.
The purpose of the Emergency Stop (ESTOP) instruction is to emulate the input functionality of a safety relay in a software programmable environment.
Available Languages
Ladder Diagram
ESTOP_LD_avail_v31
Function Block
This instruction is not available in function block.
Structured Text
This instruction is not available in structured text.
Operands
IMPORTANT:
Make sure that your safety input modules are configured as single, not Equivalent or Complementary. These instructions provide all dual channel functionality necessary for PLd (Cat. 3) or PLe (Cat. 4) safety functions.
This table explains the instruction inputs.
Operand
Data Type
Description
Safe, Active, and Initial Values
ESTOP
EMERGENCY_STOP
This operand is a backing tag. As such, it maintains important execution information for each usage of this instruction. Do not attempt to reuse this backing tag or write to any of its members anywhere else in your program.
-
Reset Type
BOOL
The reset type determines whether the instruction is using Manual or Automatic reset for Output 1.
Manual (1) or Automatic (0)
Channel A
1
BOOL
Channel A Input (Normally Open)
Safe = 0,
Active = 1
Channel B
1
BOOL
Channel B Input (Normally Open)
Safe = 0,
Active = 1
Circuit Reset
BOOL
Circuit Reset Input
Manual Reset - Sets Output 1 after Channel A and Channel B transition from Safe state to the Active state, and the Circuit Reset input transitions from zero to one.
Automatic Reset - Visible, but not used.
Initial = 0
Reset = 1
Fault Reset
BOOL
After fault conditions are corrected for the instruction, the fault outputs for the instruction are cleared when this input transitions from off to on.
Initial = 0
Reset = 1
1
If this input is from a Guard I/O input module, make sure that the input is configured as single, not Equivalent or Complementary.
This table explains the instruction outputs.
Operand
Data Type
Description
Safe, Active, and Initial Values
Output 1
BOOL
Output 1 is set to the Active state when input conditions are met.
Safe = 0
Active = 1
Cycle Inputs
BOOL
Cycle Inputs prompts for action. Before Output 1 is turned on, Channel A and Channel B inputs must be cycled through their Safe States simultaneously before the circuit can be reset.
This prompt is cleared when Channel A and Channel B transition to the Safe state.
Initial = 0
Prompt = 1
Circuit Reset Held On
BOOL
Manual Reset - The Circuit Reset Held On prompt is set when both input channels transition to the Active states, and the Circuit Reset input is already on.
The Circuit Reset Held On prompt is cleared when the Circuit Reset input is turned off.
Automatic Reset - Visible, but not used.
Initial = 0
Prompt = 1
Inputs Inconsistent
BOOL
This fault is set when Channel A and Channel B inputs are in inconsistent states (one Safe and one Active) for a period of time greater than the Inconsistent Time Period (listed below). This fault is cleared when Channel A and Channel B inputs return to consistent states (both Safe or both Active) and the Fault Reset input transitions from off to on.
Inconsistent Time Period: 500 ms
Initial = 0
Fault = 1
Fault Present
BOOL
The value is set whenever a fault is present in the instruction. Output 1 cannot enter the Active state when Fault Present is set. Fault Present is cleared when all faults are cleared and the Fault Reset input transitions from off to on.
Initial = 0
Fault = 1
IMPORTANT:
Do not write to any instruction output tag under any circumstances.
Operation
Normal Operation
This instruction monitors the states of two input channels and turns on Output 1 when the following conditions are met:
  • When using Manual Reset: both inputs are in the Active state and the Circuit Reset input is transitioned from a zero to a one.
  • When using Automatic Reset: both inputs are in the Active state for 50 ms.
This instruction turns Output 1 off when either one or both of the input channels returns to the Safe state.
Both input channels for the Emergency Stop (ESTOP) instruction are normally open. Zeros on both channels represent the Safe state, and ones on both channels represent the Active state.
These normal operation state changes are shown in the following timing diagrams.
ESTOP Manual and Reset
Operation with Inconsistent Inputs
This instruction generates a fault if the input channels are in inconsistent states (one Safe and one Active) for more than the specified period of time. The inconsistent time period is 500 ms (t1).
This fault condition is enunciated via the Inputs Inconsistent and the Fault Present outputs. Output 1 cannot enter the Active state while the Fault Present output is active. The fault indication is cleared when the offending condition is remedied and the Fault Reset input is transitioned from zero to one.
These state changes are shown in the following timing diagram.
ESTOP Operation with Inconsistent Inputs
Operation with Circuit Reset Held On - Manual Reset Only
This instruction also sets the Circuit Reset Held On output prompt if the Circuit Reset input is set (1) when the input channels transition to the Active state.
These state changes are shown in the following timing diagram.
ESTOP Operation w circuit reset held ON
Cycle Inputs Operation
If, while Output 1 is active, one of the input channels transitions from the Active state to the Safe state and back to the Active state before the other input channel transitions to the Safe state, the Cycle Inputs output prompt is set. Output 1 cannot enter the Active state again until both input channels cycle through their Safe states.
These state changes are shown in the following timing diagram:
ESTOP Cycle Inputs Operation
False Rung State Behavior
When the instruction is executed on a false rung the behavior is exactly the same as true rung state except all outputs, including prompts and fault indicators, will be zero. When the rung state becomes true the outputs will be set as determined by the instruction logic.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Index Through Arrays for array-indexing faults.
Execution
Condition/State
Action Taken
Prescan
The .O1, .CI, .CRHO, .II, and .FP are cleared to false.
Rung-condition-in is false
The instruction executes as described in the False Rung State Behavior section.
Rung-condition-in is true
The instruction executes as described in the Normal Operation section.
Postscan
The instruction executes as described in the False Rung State Behavior section.
Example
Emergency Stop with Manual Reset Wiring
The following wiring diagram is one example of how to wire a 2-channel Emergency Stop switch having two normally open contacts to a 1791DS Safety I/O module to comply with ISO 13849-1 Category 4.
ESTOP Emergency stop with manual reset
Manual Reset Programming Example
The following programming example shows how the Emergency Stop instruction with Manual Reset can be applied to the previous wiring diagram.
ESTOP_Other_Pg370_v31
ISO 13849-1 Category 4 requires that inputs be independently pulse tested. The Logix Designer application is used to configure the following I/O module operands for pulse testing.
Input Configuration
Input Point
Type
Point Mode
Test Source
0 (IN0)
Single
Safety Pulse Test
0 (T0)
1 (IN1)
Single
Safety Pulse Test
1 (T1)
2 (IN2)
Single
Safety
None
3 (IN3)
Single
Safety
None
Test Output
Test Output Point
Point Mode
0 (T0)
Pulse Test
1 (T1)
Pulse Test
2 (T2)
Power Supply
3 (T3)
Not Used
Automatic Reset Wiring and Programming
The following wiring diagram is one example of how to wire a 2-channel Emergency Stop switch having normally open contacts to a 1791DS Safety I/O module to comply with ISO 13849-1 Category 4.
NOTE:
Various safety standards (EN 60204, ISO 13849-1) require that when using the Automatic Circuit Reset feature, other measures must be implemented to make sure that an unexpected (or unintended) startup does not occur in the system or application.
ESTOP emergency stop with auto reset wiring
Automatic Reset Programming Example
The following programming example shows how the Emergency Stop instruction with Automatic Reset can be applied to the wiring diagram shown above.
ESTOP_Other_Pg371_v31
ISO 13849-1 Category 4 requires that inputs be independently pulse tested. The Logix Designer application is used to configure the following I/O module operands for pulse testing.
Input Configuration
Input Point
Type
Point Mode
Test Source
0 (IN0)
Single
Safety Pulse Test
0 (T0)
1 (IN1)
Single
Safety Pulse Test
1 (T1)
2 (IN2)
Single
Safety
None
Test Output
Test Output Point
Point Mode
0 (T0)
Pulse Test
1 (T1)
Pulse Test
2 (T2)
Power Supply
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal