Redundant Output (ROUT)

Redundant Output (ROUT)

This instruction applies to the Compact GuardLogix 5370, GuardLogix 5570, Compact GuardLogix 5380, and GuardLogix 5580 controllers.
Use the Redundant Output with Continuous Feedback Monitoring (ROUT) instruction to emulate the output functionality of a safety relay in a software programmable environment.
The Redundant Output with Continuous Feedback Monitoring Instruction can be used in two ways:
  • Redundant Output with Negative Feedback (RONF)
  • Redundant Output with Positive Feedback (ROPF)
Available Languages
Ladder Diagram
ROUT_LD_avail_v31
Function Block
This instruction is not available in function block.
Structured Text
This instruction is not available in structured text.
Operands
This table explains the instruction inputs.
Operand
Data Type
Description
Values
ROUT
REDUNDANT_OUTPUT
This parameter is a backing tag that maintains important execution information for each usage of this instruction.
Safety Advisory
ATTENTION:
To avoid unexpected operation do not reuse this backing tag and its members. Do not write to any of the tag members anywhere else in the program.
-
Feedback Type
BOOL
The feedback type determines whether the instruction is using negative or positive feedback
Negative = 0 (RONF)
or
Positive = 1 (ROPF)
Enable
BOOL
Input to Enable the Redundant Outputs
Safe = 0
Active = 1
Feedback 1
BOOL
Feedback from a device either directly or indirectly controlled by Output 1.
RONF:
Off = 1
On = 0
ROPF:
Off = 0
On = 1
Feedback 2
BOOL
Feedback from a device either directly or indirectly controlled by Output 2.
RONF:
Off = 1
On = 0
ROPF:
Off = 0
On = 1
Fault Reset
BOOL
After fault conditions are corrected for the instruction, the Fault Present output for the instruction is cleared when this input transitions from off to on.
Initial = 0
Reset = 1
This table explains the instruction outputs.
Operand
Data Type
Description
Safe, Active, and Initial Values
Output 1
BOOL
Output 1 of the redundant outputs
Safe = 0
Active = 1
Output 2
BOOL
Output 2 of the redundant outputs
Safe = 0
Active = 1
Output 1 Feedback Failure
BOOL
Output 1 Feedback is not indicating the correct state of Output 1 within 250 ms.
Initial = 0
Fault = 1
Output 2 Feedback Failure
BOOL
Output 2 Feedback is not indicating the correct state of Output 2 within 250 ms.
Initial = 0
Fault = 1
Fault Present
BOOL
This is set whenever a fault is present in the instruction. Outputs cannot enter the Active state when Fault Present is set. Fault Present is cleared when all faults are cleared and the Fault Reset input transitions from off to on.
Initial = 0
Fault = 1
IMPORTANT:
Do not write to any instruction output tag under any circumstance.
Operation
Normal Operation
This instruction monitors a single logical input and activates two field outputs when the logical input goes Active.
ROUT chart
It also monitors a feedback channel for each field output and generates a fault if both channels do not, within a time limit, indicate the desired state of the associated outputs.
Instruction operation is illustrated in the following timing diagrams:
Negative Feedback
ROUT Negative Feedback
Positive Feedback
ROUT_PosFeedback_v34
False Rung State Behavior
When the instruction is executed on a false rung the behavior is exactly the same as true rung state except all outputs, including prompts and fault indicators, will be zero. When the rung state becomes true the outputs will be set as determined by the instruction logic.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See
Index Through Arrays
for array-indexing faults.
Execution
Condition/State
Action Taken
Prescan
The .O1, .O2, .O1FF, .O2FF and .FP are cleared to false.
Rung condition-in is false
The instruction executes as described in the False Rung State Behavior section.
Rung condition-in is true
The instruction executes as described in the Normal Operation section.
Postscan
The instruction executes as described in the False Rung State Behavior section.
Example
ROUT_LD_ex_v31
Negative Feedback Wiring
The following wiring diagram illustrates how to wire two contactors, and normally open auxiliary contacts to a 1791DS Safety I/O module to comply with ISO 13849-1 Category 4.
ROUT wiring two contactors
Negative Feedback Programming
The following programming example shows how the Redundant Output instruction with negative feedback can be applied to the wiring diagram shown above.
ROUT_Other_Pg403_v31
ISO 13849-1 Category 4 requires that inputs be independently pulse tested. The
Logix Designer
programming application is used to configure the following I/O module parameters for pulse testing.
Input Configuration
Input Point
Type
Point Mode
Test Source
0 (IN0)
Single
Safety Pulse Test
0 (T0)
1 (IN1)
Single
Safety Pulse Test
1 (T1)
2 (IN2)
Single
Safety
None
Test Output
Test Output Point
Point Mode
0 (T0)
Pulse Test
1 (T1)
Pulse Test
2 (T2)
Power Supply
3 (T3)
Not Used
Output Configuration
Point
Type
Point Mode
0 (OUT0)
Single
Safety
1 (OUT1)
Single
Safety
Positive Feedback Wiring
The following wiring diagram illustrates how to wire two contactors and normally open auxiliary contacts to a 1791DS Safety I/O module to comply with ISO 13849-1 Category 4.
ROUT wiring 2 contactors and NO aux contacts
Positive Feedback Programming
The following programming example shows how the Redundant Output instruction with positive feedback can be applied to the previous wiring diagram.
ROUT_Other_Pg405_v31
ISO 13849-1 Category 4 requires that inputs be independently pulse tested. The
Logix Designer
programming application is used to configure the following I/O module parameters for pulse testing.
Input Configuration
Input Point
Type
Point Mode
Test Source
0 (IN0)
Single
Safety Pulse Test
0 (T0)
1 (IN1)
Single
Safety Pulse Test
1 (T1)
2 (IN2)
Single
Safety
None
Test Output
Test Output Point
Point Mode
0 (T0)
Pulse Test
1 (T1)
Pulse Test
2 (T2)
Power Supply
3 (T3)
Not Used
Output Configuration
Output Configuration
Point
Type
Point Mode
0 (OUT0)
Single
Safety
1 (OUT1)
Single
Safety
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal