Communications Fault
An owner controller had established a communication link with the module, but a communication problem has occurred and the link has been terminated.
module
A device, typically an I/O device, that communicates with the controller. The controller, a particular 1756-IB16I or a PanelView are all considered modules.
To recover from this fault:
- Check communication modules to make sure they are still connected to the network
- Verify that the controller is still functioningcontrollerA device that controls machines or processes elements (for example, a programmable controller or relay panel).
- Power cycle the module (if none of the above works)
Provide Feedback