Configure Alarms non-isolated analog input modules
Use the
Alarms
tab on the Modules Properties
dialog box to configure process alarms and rate alarms on non-isolated analog input modules for each channel.To configure the alarms on non-isolated analog input modules:
- SelectChannelfor the channel that you want to configure.
- In theProcess Alarmssection, enter the desired process alarm values for:
- High High
- High
- Low
- Low Low
- SelectUnlatch Allto unlatchallalarms for the channel.
- SelectUnlatchito unlatch the adjacent alarm condition.
- Use the slider bar to visualize where the process alarm trigger parts are set for your process.
- Select theDisable All Alarmscheck box ito disable alarms for the channel.
- Select theLatch Process Alarmscheck box to maintain an alarm-triggered condition for any of the process alarms after the condition ceases.
- Select theLatch Rate Alarmcheck box to maintain the alarm after the condition ceases.
- In theDeadbandbox, enter a value for which the alarm will not disable, if the input value remains within the range of the alarm trigger point.
- In theRate Alarmbox, enter a value (in Engineering Units per second), for the alarm to trigger when the rate of change between the input samples exceeds the setpoint.
- SelectApplyto save the changes and continue editing, or selectOKto save the changes and close the dialog.
Provide Feedback