Configure output limits
- In theController Organizer, right-click the module and selectProperties.
- On theModule Properties dialog, select theLimitstab.
- Select theChannelbutton to select the channel to configure.
- Enter theLimitvalues for:
- High Clamp
- Low Clamp
- Select theRamp in Run Modecheck box to enable ramping during Run mode.
- InRamp Ratebox, type the maximum rate of change that an output may make (in engineering units per second).
- Select theDisable All Alarmscheck box to disable alarms for the current channel.
- Select theLatch Limit Alarmsto maintain the high and low limit alarms after the condition ceases.
- Select theLatch Rate Alarmcheck box to maintain the rate alarm after the condition ceases.
- SelectUnlatchto unlatch the adjacent alarm condition.
- SelectUnlatch Allto unlatchallalarms for the channel.
- Use the slider bar to visualize where the process limit trigger values are set for your process.
Provide Feedback