- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Configure output limits on an isolated analog output module
Use the
Limits
tab on the Module Properties
dialog box to set clamping and ramp limits that can prevent damage to equipment.To configure the output limits on an isolated analog output module:
- In theController Organizer, right-click the module and selectProperties.
- On theModule Properties dialog, select theLimitstab.
- Select theChannelbutton to select the channel to configure.
- Enter theLimitvalues for:
- High Clamp
- Low Clamp
- Select theRamp in Run Modecheck box to enable ramping during Run mode.
- InRamp Ratebox, type the maximum rate of change that an output may make (in engineering units per second).
- Select theDisable All Alarmscheck box to disable alarms for the current channel.
- Select theLatch Limit Alarmsto maintain the high and low limit alarms after the condition ceases.
- Select theLatch Rate Alarmcheck box to maintain the rate alarm after the condition ceases.
- SelectUnlatchto unlatch the adjacent alarm condition.
- SelectUnlatch Allto unlatchallalarms for the channel.
- Use the slider bar to visualize where the process limit trigger values are set for your process.
- SelectApplyto save the changes and continue editing, or selectOKto save the changes and close the dialog.
Provide Feedback