Major Recoverable Fault
A communication fault has occurred in an analog module. The module lost a connection with the controller. A digital module does not have major recoverable faults.
If the software configuration and the actual physical hardware differ greatly (such as, the software has been configured for a digital module and the actual physical module is an analog module), then the software can only display this generic status:
- Unrecoverable Fault
- Recoverable Fault
- None
Access the
Connection
tab on the Module Properties
dialog box for more information about a module fault.Provide Feedback