Select Channels to Calibrate
To select channels to calibrate:
- Select theCalibrate?box for each channel that you want to calibrate.
- Select the desired method of calibration button (GroupsorOne at a Time).You can calibrate channels in groups at the same range simultaneously, or one at a time. When you calibrate channels one at a time, you go through a complete calibration on a per channel basis before moving onto calibrate the next channel.
- Select:
- Backto return to the previous screen.
- Nextto continue.
- Stopto cancel the calibration.
Provide Feedback