Failed to acknowledge positive Rate of Change alarm

Problem attempting to acknowledge the
Positive Rate of change
alarm. The error indicates one of these conditions.
Acknowledgment not required for this alarm
Cannot acknowledge an alarm that does not require acknowledgment. Check
Acknowledgment Required
in the Configuration dialog box to require the acknowledgment.
This alarm has already been acknowledged
Cannot acknowledge an alarm that was already acknowledged.
Acknowledged with wrong parameters
Invalid parameters were sent with the acknowledge command.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.