Guidelines to drag between organizers

Guidelines to drag between organizers

You may want to drag-and-drop an item between the
Logical Organizer
and the
Controller Organizer
. If the two organizers are "stacked," all that is visible for the second organizer is the tab at the bottom of the organizer window. To drag-and-drop an item to the other organizer, drag the selected item to the tab for the other organizer. After a second or two, the other organizer appears and you can continue to drag the item to the target item.
Organizer_tabs.jpg
These are the restrictions for drag-and drop items in
Controller Organizer
:
  • You cannot drag a Safety item when in Safety Lock. If you select multiple items, and any of them is a Safety item, you cannot drag-and-drop any of the selected items in Safety Lock.
  • You cannot use drag-and-drop operations if the system is in Hard Run or has a major fault.
  • You cannot paste a program if doing so would exceed the limit of 1000 child programs at the target item, or if it would exceed the limit of 1000 programs scheduled under a task.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal