Controller Organizer icons

The
Controller Organizer
window contains a hierarchy of the folders, files, and links that contain all of the information about the programs and data in the current project. The following table lists the icons that appear in the
Controller Organizer
.
Icon
Description
Icon
Description
RSL5K_OpenFolderIcon_v31
Open folder
RSL5K_SafetyTaskIcon_v31
Safety task
RSL5K_ClosedFolderIcon_v31
Closed folder
RSL5K_SafetyProgramIcon_v31
Safety program
RSL5K_TagsFolderIcon_v31
Tags folder
RSL5K_SafetyAOIIcon_v31
Safety Add-On Instruction
RSL5K_ContinuousTaskIcon_v31
Continuous task
RSL5K_SealedAOIIcon_v31
Sealed Add-On Instruction
RSL5K_PeriodicTaskIcon_v31
Periodic task
RSL5K_SealedSafetyAOIIcon_v31
Sealed safety Add-On Instruction
RSL5K_ProgramIcon_v31
Program
RSL5K_MainSafetyLadderIcon_v31
Main safety ladder routine
RSL5K_AlarmIcon_v31
Alarms
RSL5K_OpenDatatypeFolderIcon_v31
Data type folder open
RSL5K_AOIIcon_v31
Add-On Instruction
RSL5K_ClosedDatatypeFolderIcon_v31
Data type folder closed
Ladder icon
Ladder routine
RSL5K_DatatypeIcon_v31
Data type
RSL5K_MainLadderIcon_v31.png
Main ladder routine
RSL5K_TrendIcon_v31
Trend
RSL5K_FBDIcon_v31
Function block routine
IO_ConfigFaultOpen_v31
I/O Configuration fault open (shown online when any module is faulted)
RSL5K_SFCRoutineIcon_v31
Sequential function chart routine
IO_ConfigFaultClosed_v31
I/O Configuration fault closed (shown online when any module is faulted)
RSL5K_StructuredTextIcon_v31
Structured text routine
backplane_v31
Backplane
RSL5K_PhaseIcon_v31
Equipment Phase
module_v31
Module
RSL5K_EquipmentSequenceIcon_v31
Equipment Sequence
faultedModule_v31
Faulted module
RSL5K_LockedRoutineIcon_v31
Locked routine
safetymodule_v31
Safety module
RSL5K_LockedAOIIcon_v31
Locked Add-On Instruction
Ethernet_v31
Ethernet
RSL5K_LadderPhaseStateIcon_v31
Ladder phase state routine
NetlinxCommCard_v31
NetLinx communications card
RSL5K_FBDPhaseStateIcon_v31
Function block phase state routine
coordinateSystem_v31
Coordinate system
RSL5K_SFCPhaseStateIcon_v31
Sequential function chart phase state routine
Axis_v31
Axis
RSL5K_StructuredTextPhaseStateIcon_v31
Structured text phase state routine
LogicalOrganizerLink_v31
Link to the Logical Organizer
For additional information about the
Controller Organizer
, see:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.