Step states in an Equipment Sequence

When a step is not active, the step state is inactive. When a step is active, and attached to an Equipment Phase, the step state mirrors the state of the Equipment Phase. The step state is also represented by the color of the step.
Steps listed as
No Phase
only have two displayed step states: RUNNING and IDLE.
Step States
Description
ABORTING
ABORTING means the
Equipment Phase
's ABORTING routine is executing.
ABORTED
ABORTED means the
Equipment Phase
's ABORTING routine is finished.
HOLDING
HOLDING means the
Equipment Phase
's HOLDING routine is executing.
HELD
HELD means the
Equipment Phase
's HOLDING routine is finished.
RESETTING
RESETTING means the RESETTING logic is executing.
RESTARTING
RESTARTING means the RESTARTING routine is executing.
RUNNING
RUNNING means the RUNNING routine is executing.
STOPPING
STOPPING means the STOPPING routine is executing.
STOPPED
STOPPED means the STOPPING routine is finished.
COMPLETE
COMPLETE means the RUNNING routine is finished.
IDLE
IDLE means the step is active and attached to the associated
Equipment Phase
, but the
Equipment Phase
is not executing a routine.
INACTIVE
INACTIVE means that the step is not active and is not attached to its associated
Equipment Phase
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.