Create an Equipment Sequence program
Equipment Sequence
programs:- Describes the order in whichEquipment Phases run and when they are started and stopped.
- Run as a program containing only one routine—the sequence diagram.
- Use sequence input parameters and sequence output parameters.
- Displays the same states as a phase. The current state is based on active sequence elements.
Add steps, transitions, links, divergent and convergent branches to manually construct
Equipment Sequence
s. Equipment Sequence
s are created in either simple series, loop, simultaneous, or selective structures. To create
Equipment Sequence
programs- Define a newEquipment Sequence.
- ConfigureEquipment Sequenceproperties.
- ConstructEquipment Sequencediagrams. SeeEquipment Sequence Diagrams.
- Create a Sequence Parameter using theNew Parameter or Tagdialog.
Provide Feedback