Generate Signature Report command
Choose this command to generate a safety signature report that shows when each safety element last changed. The most recent changes are highlighted in a style similar to the Compare Tool.
The generated safety signature report is displayed in a Web browser. A copy of the safety signature report is also saved in this folder:
C:\\Users\Public\Documents\Rockwell Automation\Studio 5000\Logix Designer\Safety Signature Reports
The file name of the saved safety signature report is comprised of the project name and current date and time.
For a complete overview of safety signature elements, see the ControlLogix 5580 and GuardLogix 5580 Controllers User Manual.
Provide Feedback