Change Ladder Editor preferences

In
Workstation Options
, use the
Ladder Editor
category to configure the options available in the Ladder Editor.
To change Ladder Editor preferences
  1. Select
    Tools
    >
    Options
    to open
    Workstation Options
    .
  2. Select the
    Ladder Editor
    category.
  3. To use hot keys for ladder editing, select the
    Enable Quick Key
    check box.
  4. If
    Enable Quick Key
    is selected, select
    Show Quick Key Configuration
    to display quick key configuration.
  5. To configure Quick Keys, select
    Configure
    .
    Quick Key Configuration
    opens to assign Quick Keys.
  6. To automatically audit edited ladder logic, select
    Enable Auto Rung Verification
    . Any errors found display in
    Output
    .
  7. Select
    OK
    to close
    Workstation Options
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.