Failed to start a pending rung edit for rung # <Rung Number>
Failed to start a pending rung edit for rung #<Rung Number>. This could occur because:
- the rung number is not a valid rung number in the routine
- the rung at the rung number is not a rung on which a pending edit can be started
- the routine was deleted
Provide Feedback