PAH labels and decimal places

PAH labels and decimal places

Use the
HART configuration
tab on the
PAH Properties
dialog box to enter input labels, unit labels, and decimal place settings for Process Analog HART (PAH) instructions.
To enter input labels, unit labels, and decimal place settings for PAH instructions
  1. On the instruction in the routine, perform one of these actions:
    • On the Ladder or FBD instruction, select .
    • In the Structured Text editor, right-click the tag name and select
      Configure <tag name>
      .
  2. Under the
    HMI
    tab, select
    HART configuration
    .
  3. Configure these settings:
    • HART variable decimal places
      . The number of decimal places displayed on the HMI for the associated HART variable.
    • HART variable labels
      . The label displayed on the HMI for the associated HART variable.
    • Enable use of the text configuration from the HART device
      . Enable use of the text configuration from the HART device for analog and digital signal units.
    • Digital signal engineering units
      . The engineering units displayed on the HMI for the associated HART variable when not using the text configuration from the HART device.
  4. Monitor these parameters:
    • The
      Digital signal HART units
      column displays the units from the HART device that are displayed if the instruction is configured to use text configuration from the HART device.
  5. When online with the controller, monitor the
    Device state
    and
    Device issues
    indicators at the bottom left of the dialog box:
    • Device state
      . Displays the current device state, such as
      Live
      ,
      Diagnostic information
      , or
      Maintenance required
      .
    • Device issues
      . Displays fault conditions, such as
      HART communication lost
      or
      Module connection fault
      .
  6. Select
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal