Alarm conditions for PVSD

Use the
Alarms
tab on the
PVSD Properties
dialog box to assign settings to pre-defined alarms for the Process Variable Speed Drive (PVSD) instruction.
Define alarm conditions for PVSD instructions
  1. On the instruction in the routine, perform one of these actions:
    • On the Ladder or FBD instruction, select .
    • In the Structured Text editor, right-click the tag name and select
      Configure <tag name>
      .
  2. Select
    Alarms
    .
  3. Set the parameters:
    • Use
      . Select the check box to put the associated alarm in use. Alarm driving conditions are not evaluated when the alarm is not in use. The
      Use
      check box is synchronized with the
      Use and evaluate alarm
      check box in the
      Alarm Properties
      dialog box.
    • Alarm.
      Type the label to be displayed for the alarm.
    • Edit button
      . Select to open the
      Alarm Properties
      dialog box for the alarm instance.
    • Apply following settings to all alarms
      . Select the check box to apply settings (Class, Alarm group, FactoryTalk View command) to pre-defined alarms for the instruction. It is important to add information to all three settings when applying alarms. If one of the settings is empty, the settings are cleared in all alarms. When changes are applied, the settings and the check box are cleared.
    • Class
      . Use classes to group related alarms. The class applies to all pre-defined alarms for the instruction. Use the class only to filter the alarms that are displayed to the operator. The class is case-sensitive.
    • Alarm group
      . Assigns pre-defined alarms for the instruction a group name to help classify and sort alarms.
    • FactoryTalk View command
      . A command that can be run on the operator station when the alarm notification appears. Type the exact syntax for the
      FactoryTalk View
      command. The command applies to all pre-defined alarms for the instruction.
    • Allow operator to shelve alarms
      . Select the check box to allow the operator to shelve alarms.
    • Allow maintenance to disable alarms
      . Select the check box to allow maintenance to disable alarms.
  4. View read-only parameters:
    • State
      . The state of the alarm. Hover over the state icon to see a tool tip that describes the alarm state or fault status.
      An alarm can be in more than one state at a time. For example, an alarm can be in alarm, acknowledged, and suppressed; or normal, unacknowledged, and suppressed.
      Alarm state icons include:
      • Normal, acknowledged (no icon).
      • Normal, unacknowledged - NormalAlarmUnacknowledged
      • In alarm, acknowledged - InAlarmAcknowledged
      • In alarm, unacknowledged - InAlarmUnacknowledged
      • Suppressed - AlarmSuppressed
      • Shelved - AlarmShelved
      • Disabled - Alarm Disabled icon
      • Alarm fault - AlarmFault
    • Device state
      . When the
      Logix Designer
      application is online with the controller, the indicator displays the current device state, such as Stopped, Running, or Out of service.
    • Device issues
      . When the
      Logix Designer
      application is online with the controller, the indicator displays fault conditions, such as Drive fault or I/O fault.
  5. Select
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.