Delete a task

Delete a task

Each task contains the programs that it executes. To delete the task,first unschedule each program.
Safety tasks cannot be deleted.
To delete a task:
  1. Unschedule each program under the task.
  2. Select the task in the
    Controller Organizer
    .
  3. From the
    Edit
    menu, choose
    Delete
    .
  4. When the confirmation dialog appears, click
    Yes
    to delete the task.
    The task no longer appears in the
    Controller Organizer
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal