The attempted command cannot be executed because it would cause overtravel condition
This command would cause overtravel if completed. Move the axis away from the overtravel condition and then retry the command.
Provide Feedback