- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Save a trend log
The
Save Trend Log As
dialog box lets you save the log working file to a file on your hard drive that you can reference at a later time.To save a trend log:
- InFile Name, enter the name of the file.
- From theSave as Typepull-down menu, choose the.TBSfile type to save the log in a format that can be opened in theLogix Designerapplication, or choose.CSVto save the file as a comma-separated value text file.
- Select theSave All Capturescheck box to save all captures in the log working file.Clear this check box and enter values inStart timeandStop timeto save only captures that occurred within that time period.
- Select theSavebutton to save the file to the name and location you specified.
Provide Feedback