Delete a trend
There are three ways to delete a trend from the Controller Organizer:
- Select the trend you wish to delete and then press the Delete key.
- Select the trend you wish to delete and then selectEdit>Deletefrom the main menu.
- Right click the trend you wish to delete and chooseDelete.
When attempting to delete a trend, you are prompted to confirm the deletion. In the confirmation dialog , select
Yes
to remove the trend from the controller or select No
to cancel the operation.Deleting a running trend causes the trend to be stopped and then deleted.
Provide Feedback