By Jon D. Miller, technical compliance manager, Det-Tronics
Editor's Note: This article is adapted from a white paper, "Gas safety standards are changing in 2020: Will your plant be in compliance?" Download the free, full white paper with additional information about what the changes mean for high-hazard process owners; other relevant codes and standards in transition that will impact selection and installation of gas detection equipment; and benefits of integrating gas detection with fire and smoke detection as a risk mitigation strategy.
Combustible and toxic gas detection is one of the first lines of defense in plant safety, and hazardous process operators understand its critical role in risk mitigation. Soon, however, existing equipment and practices for gas detection may no longer suffice. Significant changes to standards are coming soon — and the best way to verify compliance will be to select, specify and install an integrated fire and gas safety system that will meet the expected 2020 standards.
IEC Updating Combustible Gas Safety Standards
Activity aimed at modernizing and unifying applicable codes and standards has been notable in the area of gas safety systems. One combustible gas related IEC (International Electrotechnical Commission) standard recently released is IEC 60079-29-1:2016, “Explosive atmospheres — Part 29-1: Gas detectors — Performance requirements of detectors for flammable gases.”
The latest edition of this standard specifies general requirements for the construction, testing and performance of fixed gas detectors intended for use in explosive atmospheres, such as those found in petrochemical and hydrocarbon processing facilities. The update adds significant new criteria in four areas, as follows.