Machine and equipment builders can give end users access to more production information and help them work more efficiently using the latest version 7 release of the Studio 5000 View Designer software. Rockwell Automation has updated the design environment for its PanelView 5000 family of operator terminals to improve how production workers do their jobs.
The software now includes an alarm history viewer that stores and provides access to up to 40,000 alarm transitions. This can help operators and technicians more quickly identify the root cause of problems like shutdowns. Workers can sort and filter alarm data and open a details pane to see more information about individual alarms. They can also export an alarm history to an SD card or USB drive for external analysis.
New configurable screen update rates allow screens and pop-ups to be configured to update as often as every 100 milliseconds – five times faster than was previously possible. This can help operators better know if machine movements are following expected motion profiles. It can also create smoother movement of on-screen animations like rotating fans.
The latest version of the software also includes a larger keypad and keyboard option. This can create easier and more efficient touch interactions for operators, especially those who wear gloves.
The Studio 5000 View Designer software provides an intuitive, modern design environment for PanelView 5000 operator terminals. Integration between Logix control systems and the terminals also improves programming efficiency and runtime performance.
PanelView, Studio 5000, Studio 5000 View Designer and Rockwell Automation are trademarks of
Rockwell Automation Inc. Trademarks not belonging to Rockwell Automation are property of their respective companies.
Published October 25, 2020